Editing a Scenario

This procedure guides you through the settings to edit a scenario using the Scenario Generator node on the software's user interface (UI). To learn more about individual cell settings, refer to the UI descriptions.

Editing a scenario applies only to stored scenario files.

To view a list of the completed edits through the UI, see the log at the bottom of the view in the Scenario Graphics node.

  1. In the tree node, click Scenario Generator .

    Notice that the software starts with Create as the default Generation Mode.

  2. Click Generation Mode, and from the drop down menu, select Edit.

  3. View the Comment cell and if desired, enter a new comment or modify an existing comment.

    If a comment was entered into the Comment cell during the scenario creation, that same text appears in the Edit mode.

  4. Click the Source Scenario File cell, and use the dialog box button to launch the Open dialog box for navigating to and selecting the scenario file to edit.

  5. If there is a desire to keep track of the edits, click the Save Edit Log cell, and from the drop down menu, select  On.

    The software saves the log file with the same name (uses .log extension) and at the same location as the edited scenario file when you click the Save Scenario button.

  6. Click Edit Mode and from the drop down menu, select the mode:

  7. Finish configuring the settings for the selected Edit Mode:

  8. To make further edits using another mode, repeat Steps 6 and 7.
  9. When all changes have been made, click the Save Scenario button to launch the Save As dialog box for selecting a location and saving the file.

Scenario Generator